Part Number: LMH0324
Other Parts Discussed in Thread: LMH0318, , LMH1218EVM, LMH1218, LMH1219EVM, LMH1219
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I'm planning on developing a HD-SDI 2:1 switch using 2 x LMH0324 and 1 x LMH0318.
The customer has a requirement of 16ms latency through the switch and a switching time between inputs of 160ms.
I cant see any relevant data in the datasheets for the LMH0324 and LMH0318.
1) What is the switching speed of the input mux on the LMH0318 ?
2) What delay/latency does the video signal experience when routing through the LMH0324 and LMH0318 ?
3) As the evaluation module for the LMH0318 is no longer available can I use the LMH1218EVM as an evaluation module for the LM0318, if so do I need to replace the LMH1218 device on the board ?
4) Similarly can I use the LMH1219EVM to evaluate the LMH0324, again by swapping the part?
Thank you for your support!
Regards,
Danilo