Part Number: DS90UB941AS-Q1
Hi Team,
My customer will use 2:2 independent mode with output DSI_PORT_SEL option.

So DSI port 0 would be output to Link lane 1 and DSI port1 would be output to Link lane0.
And T_skip setting should be set on each port respectively.
so My customer questioned ifT_skip setting for DSI port0 is also changed to port1 according to swap option.
e.g, if 27MHz input to DSI port 0 and output is Link lane1, customer need to set Tskip on DSI port1 not DSI port0??
I believe Tskip setting doesn't need to follow DSI_PORT_SEL option.
Could you pls confirm this??
Thanks