This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1EVM: DS90UB954-Q1EVM

Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: DS90UB953-Q1EVM, , DS90UB960-Q1EVM

Hi

Is it possible to stream MIPI-CSI2 cameras thorough DS90UB954-Q1EVM evaluation board to DS90UB953-Q1EVM?

I am using Allied vision MIPI cameras. Please advise how to achieve this. it can be even ds90ub960-Q1EVM. however it seems to be not available. please advise how can I get it if avilable?

I am looking to stream my prototype thorough FPD-LINK using any off the shelf evaluation modules available for FPD link

  • Hi Mojtaba,

    It is possible to stream MIPI-CSI2 cameras through the 954 EVM board to the 953 EVM board.

    The 954 is a dual deserializer hub, which can receive data input from two compatible serializers (over the FPD-Link III interface) and then aggregate the data to a CSI-2 output port. The 953 EVM can be connected to that CSI-2 output port to receive the aggregated data.

    Some notes to consider if you are planning on using the 954 EVM.

    1. The 954 EVM has two Rosenburg FAKRA connectors installed and is setup for two COAX connections, by default.
    2. The RX0 port is connected to AC coupling capacitors and a PoC circuit, which is suitable for connection to a 953 EVM.
    3. The RX1 port has components installed, which make it suitable for connection with a 933 EVM. 
      1. You can add/remove components to make RX1 port suitable for a 953 connection.

    Best,

    Justin Phan