Part Number: DS280DF810EVM
I have DS280DF810EVM. When I use it to generate PRBS and check the eye on a DCA I only have an amplitude of 395mV. That is really low. I'm using Sigcon. I have try different setting for the ''transmitter FIR/VOD settings'' I can lower the signal but can't go over 395mV at 25 Gbps. If I lower the data rate, I have little more amplitude, but still low.