Part Number: DS90UH948-Q1
Hi,
we plan to use a Dacar 636-2 cable with a M12 x-coded connector over an distance of 10m. The transmitter will be a DS90UH949A.
Is it possible over a distance of 10m?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH948-Q1
Hi,
we plan to use a Dacar 636-2 cable with a M12 x-coded connector over an distance of 10m. The transmitter will be a DS90UH949A.
Is it possible over a distance of 10m?
In addition: The display resolution is 1400x1050@60Hz and Dual OpenLDi is used.
Hello Oliver,
Yes, 10m cable is possible for your configuration, if you can keep the Board Insertion loss as per our recommendations.
The counterpart (transmitter side) has confidential information from Ti and is telling us and the other involved parties, that the cable length is limited to 6.7m because of insertion loss, inter pair shew and intra pair skew.
We are not able to check this, because we do not have this confidential information from Ti. (The mentioned information may be linked to DS90UB949A)
The 949A is the transmitter!
Can you share with me more details? Which counterpart do you mean? If the details are under NDA, please send me an email or Personal Message in this forum.
Can you provide me an email for a private message? The problem is quiet complicate and I am already tried to address this to Ti in German