Part Number: DS90UB941AS-Q1
Hi Casey,
I have a question would like to consult with you. Currently customer uses DSI clock as the 941 reference clock, but customer faces a problem that is, when the DSI controller on the SOC side does not output the clock, the FPD-LINK 3 of the 941AS cannot work normally, which means the SOC side cannot see the address of the touch IC after the 948 on the I2C bus, and cannot initialize the touch IC.
Their current solution is to use the internal clock of 941 to make the FPD-LINK3 work normally before the DSI clock on the SOC side came, so that the touch IC can be initialized normally. Does this operation have potential risks? Could the internal clock of 941 ensure stable i2c communication? Thank you!