Part Number: DS90UB941AS-Q1
Dear TI:
The ser-des connection is: host dsi->ub941->ub948->display
We met one issue. The display work abnormal in the following sequence:
1. system boot up
2. Host dsi & UB941 init
3. Do not UB948 initial work until UB948 is plugged in mannually(after 5 minutes).
Then the display is abnormal. Do it need to configure UB941 again when configuration UB948? Can you provide some example configuration? Thanks.
BRs,
Arvin