This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9555: Can the external pull up resistor not used?

Part Number: TCA9555

Hi team, 

A quick question, can we just use the internal 100kohm for pull up and not use the external pull-up resistor if we can limit the output current for P07-P00 and P17-P10 below 80mA each and 160mA total ?

Thanks

  • Hi Reagan,

    Yes, it is fine to rely on the 100k-ohm internal pull-up for the input pins. Make sure you consider the leakage paths that exist external to the device and the relatively slow rise-time of the signal if the signal driver goes high impedance from an output-low state (such as an open-drain output). 

    Note that this only really applies when the pin is configured as an input, as the pin will be push-pull while configured as an output. 

    Regards,
    Eric Schott

  • Hi Eric,

    Noted. Thanks for your detailed comments!