Part Number: DP83867E
Hello, I am using the DP83867E on my custom board and we have unintentionally put RX-CTRL strapping pin in only Mode 4. This will disable Auto Negotiation. I need to put the pin in Model 3 but unfortunately I did not put in the design for Rlo.

I was looking over page 38 in the data sheet and it has the following:

When I go to page72 to look at the Configuration Register bit 7 it shows:

Bit 7 is shown to be Reserved and the default value is 0.
Does this mean the device will set Auto Negotiation to be enabled?
Thank you
Joe