Other Parts Discussed in Thread: DRV8825, TPS2660, TPL1401
Hi All,
We have to control the DRV8825 stepper motor driver by MCU. That is the interface. Also we have to control RCD-24-1.20 LED driver by I2C programming through a DAC. Here, we are connecting different color combination of 5-6 high current LED bundle on the output of above mentioned LED driver. We have rotational device setup which will connect the various combination of LEDs(color) bundle with this single LED driver. There fore this maximum current is changing in that LED line. we have to include a over current protection circuit on that LED line like a fuse to protect LEDs. but notice that the maximum current on this line is changing. There fore we can not proceed with fuse. we are looking for a solution for above mentioned problem. Do we have any IC that are protecting a line from over current and rated current can be programmed through any interface?