This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064: USB3.0 interference DP lead OLED flash when TUSB1064 use as 2 lane DP and 2 lane USB3.0

Part Number: TUSB1064


Hi TI,

Our produc is VR device that use tusb1064 as MUX;2lane DP run 8.1Gbps transmit 3840*1920@60Hz image,2lane USB 3.0(gen1)transmit camera UVC.when we connect our device to computer,OLED of our device start to flah badly,TUSB1064 setting DP EQ =10dB  USB3.0=10dB if we adjust less USB 3.0EQ to 0.7dB,flash of OLED can lighten,if we remove USB3.0 connect in hardware ,OLED will not flash;

Why USB3.0 interference  DP?How to fix it? thanks!