Part Number: TVS3300
Hello Team,
is it possible to put two or more TVS330x in series to get a higher clamp voltage?
Thanks
Jan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jan,
In theory, this could work. However, we have not tested our devices for this scenario, so we can't guarantee a specific voltage. I'm assuming you mean Vrwm and not clamping voltage.
Regards,
Matt Smith
Hi Matt,
thank you for the quick answer. My customer builds a servo drive board and want to protect the mosfets against surge. The application of their customers is typically battery driven 48V. They can have voltages up to 80V on the motors. The customer talked about clamp voltage, but I think he meant Vrwm. Do we have another solution for this type of application?
Thanks
Jan
Hi Matt,
one update from the customer. You were correct- they looked for Vrwm ~ 65V and they now ordered samples and will try to put two flat clamp diodes in series. The case that they try to cover here is not a battery applied application. They look into the case when their servo drive will be supplied via a long wire. The current that can flow through this wire can be up to 45A peak at 60V.
Do you have any concerns with putting to diodes in series?
If have a better concept for protecting against surge in a 60V application let me know.
Regards
Jan
Hi Jan,
Probably the biggest thing that the customer will notice is that the clamping voltage (ie. the voltage the system receives during a surge event) will be much higher since there will be more resistance on the line with the 2 devices as opposed to 1. This is the only solution we have for this working voltage right now since our highest Vrwm in our portfolio is 33 V with TVS330/1. Please keep me posted on what the customer's results are when they test this.
Regards,
Matt Smith