Other Parts Discussed in Thread: SN65LVDS31, SN65LVDS33, SN65LVDS179-EP, SN65LVDS051-Q1, SN65LVDS050-Q1
I am looking for an EP (or SEP) LVDS driver & receiver combination for use with the SpaceWire protocol, which needs 2 x 400Mbps driver and 2 x 400 Mbps receiver per port. The prototype uses SN65LVDS31 and SN65LVDS33 parts in TSSOP16 packages, which are also available in EP - BUT the EP devices are in the much larger SOIC16 packages. This is not convenient for my multi-port design.
I came across the SN65LVDS179-EP, whose datasheet specs a SN65LVDS050-EP in TSSOP16, but this is not listed in the December-2020 orderable devices table. Also the 179 family does not have the common mode input tolerance that originally attracted me to the 33.
Does there exist a useful device for me to consider in TSSOP16 or smaller with EP, SEP, or at least AEC Automotive, rating?
Many thanks for your attention.