Part Number: SN65DSI84
Other Parts Discussed in Thread: DSI-TUNER
Hi Sir,
Our company is now working on an RFI project,
Its core will use NXP i.MX8M mini ARM processor,
We planned to use SN65DSI84ZXHR to convert MIPI-DSI to LVDS to connect to LCM module.
System will use Linux base OS in future.
Please help check the following questions and provide comment, thanks.
1). Is there a firmware code inside SN65DSI84ZXHR IC?
2). Can SN65DSI84 adjust the display setting register through the I2C bus which is connected to the processor?
3). Will TI provide software support for Linux driver in the future?
4). Is the TI DSI-Tuner utility can support Linux OS?