Part Number: DS280BR810
Dear Support team,
Data sheet P.17 states "Maximum EEPROM size is 8 kb (1024 x 8-bit)."
In recent years, smaller memory size EEPROMs have been difficult to obtain.
I am considering using an EEPROM that exceeds the capacity (e.g., 128kb or 256kb parts). Are there any problems with the use?
According to Figure 5 in datasheet, there is a description of " 8-bit SMBus address: 0xA0 ".
7bit_address [1010000] + Read/write select [0] = [10100000] = 0xA0 at 8bit
Is it correct?
Best Regards,
Hirokazu Takahashi