Part Number: DP83848-EP
The DP83848 has Application Note AN-1469 which covers its layout guidelines.
In Section 4, it is mentioned that 0.1μF decoupling capacitors should be placed as close as possible to the Vdd pins (the device has 3 - AVDD33, IOVDD33_1 and IOVD33_2). However, for the 10μF bulk capacitor, it is mentioned that it should be placed close to the PHY in general. Is it advised to place the bulk capacitor close to any particular Vdd, say the pin which draws the most current during normal operation ?