Part Number: DP83848-EP
The DP83848 has Application Note AN-1469 which covers its layout guidelines.
In Section 5, it is mentioned that the MII Signals shall have 68Ω characteristic impedance (which is in compliance with the IEEE 802.3u standard). However, I was unable to find any recommendations for the characteristic impedance for the Station Management Signals (MDIO and MDC). Is there any such recommendation for these signals from TI ?