Part Number: TUSB321
Hey Expert,
I am looking for an USB component TUSB321, can you help clarify the application of this chip and USB nego mechanism when plugging a PD device with 9W consumption, thanks for support.
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB321
Hey Expert,
I am looking for an USB component TUSB321, can you help clarify the application of this chip and USB nego mechanism when plugging a PD device with 9W consumption, thanks for support.
Jim
Hi Jim,
TUSB321 is a CC controller and should be used for application that do not require greater than 15W of power over the USB-C connector. Please refer tot eh FAQ linked below for more details.
When a PD controller is connected USB-C termination is presented but no PD messaging will occur.
Hey Malik,
Thanks for reply.
Jim