This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9617A: Finding a Level Shifter which fits to TCA9617A (1MHz)

Part Number: TCA9617A
Other Parts Discussed in Thread: PCA9306, TCA9406, TCA9416

Hey,

I've got an I2C design which runs at Super Speed Plus (1MHz). At some point it has an TCA9617A.

The B Side (3.3V) is connected to a cable of 10 inch to another pcb. At this I've got an I2C Bus running at 1MHz 1.8V.

Do you know any Buffer/Level Shifter which is able to fullfill the requirements of connecting both busses? I2C Buffers runnning at 1 Mhz are pretty rare. And these which are available consists of a B side with a static voltage offset. So a B side cannot be conntected to another B side. But all B sides starts at a voltage of 2.2V... so I cant use the B side at the 1.8V side.

I thought about using a level shifting switch as well (like PCA9306), but these seme to be incompativle with the B sides as well.


                                      3.3V
       Aside                     Bside                  3.3V                 1.8V
       ┌────────────┐               ┌────────────┐
       │  TCA9617A               ├─────┤                     ?????    │
       │  1MHz                         │               │                       1MHz    │
       └────────────┘               └────────────┘

Thanks a  lot for your support!

Nicolai