This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2046B: Crystal required for the USB hub

Part Number: TUSB2046B


In the datasheet, recommended crystal load capacitance = 20pF and value of C1 and C2 = 27pF. We have designed our circuit with this recommendation. However, due to the recent part shortages, we are not able to find a crystal with 20pF load capacitance. Only available crystals are with 10pF capacitance. So, my question is will the  Crystal with 10pF capacitance work? with C1 and C2 = 15pF? Or what would be recommended value for C1, C2 with 10pF crystal load capacitance?