This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25810: Is TPS25810 the right choice for this dock?

Part Number: TPS25810


As shown in attached picture: the original dock is very simple.

Now the dock would be modified for accessing Ethernet via an USB to Ethernet controller and being charged simultaneously. Is it possible to make it happen? Because I am worrying about that Android device is sourcing current when it is working with USB to Ethernet controller as a host,  if there is current from charging adaptor/computer/tablet, will  they be conflict? Any IC could solve this?

Thanks.