Part Number: DS90UB954-Q1
Expert,
Why we have RAW12 HF/LF mode for DS90UB954? When should I select HF vs. LF mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB954-Q1
Expert,
Why we have RAW12 HF/LF mode for DS90UB954? When should I select HF vs. LF mode?
Hello Ryan,
these modes shall be used only when paired with a parallel SER such as UB913A or UB933.
RAW12LF supports max. PCLK of 50MHz, and RAW12HF supports PCLK of max 75MHz.
Hamzeh,
RAW12HF can also support PCLK 50MHz, right? What's the benefit we choose LF for 50MHz PCLK?
Great thanks
It is recommended to use RAW12LF for PCLK from 37.5MHz to 50MHz, and use the RAW12HF from 51MHz to 75MHz.