Part Number: TVP5150AM1
Other Parts Discussed in Thread: TVP5150
Hi,
My customer have below question for TVP5150AM1.
The camera they used as below.

They have use other decode IC can normal work, but output pixel clock to high so can't use in this case,
Now used TVP5150, but input signal can't decode and suspect is input vp-p issue,
ntsc input vp-p measurement value about 1.8vp-p, is it over TVP5150 0.75V so can't use?
Is any way to low down signal level to solve this issue? Can used level shift IC to solve it?
Thanks!