Part Number: LMH0303
HI Team.
i found below description in datasheet 7.3.5. So if we want to enable the cable detection function, we need to pull-up the enable pin firstly, right? And if we pulled-down the enable pin, the cable detection function can't work, right?
The cable driver must be enabled for the termination detection to operate. If the termination fault will be used to
power down the LMH0303, then periodic polling (enabling) is recommended to monitor the output termination.
For example, when a fault condition is triggered, ENABLE can be driven low to power down the device. The
LMH0303 should be re-enabled periodically to check the status of the output termination. The LMH0303 must be
powered on for at least 4 ms for termination fault detection to work.