Part Number: TUSB4041I
Hi,
We use tusb4041i chip on our board, and find a issue.
If the downstream ports does not insert any USB device, and then insert a USB device, the USB host controller will no longer be able to detect this device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB4041I
Hi,
We use tusb4041i chip on our board, and find a issue.
If the downstream ports does not insert any USB device, and then insert a USB device, the USB host controller will no longer be able to detect this device.
Hi,
If you power on with a device connected on the downstream port, does it work? If you are using Linux or Android, can you update your build? The host controller not responding to the interrupt endpoint of the hub was a problem with some very early builds.
Regards,
JMMN
Thank you for your reply.
--If you power on with a device connected on the downstream port, does it work?
Yes, it can work, and other ports can detect the inserted device.
--If you are using Linux or Android, can you update your build? The host controller not responding to the interrupt endpoint of the hub was a problem with some very early builds.
We use the Linux 4.19, is a relatively new version. How old is the very early version you said?
Thanks.
Hi Wei,
It sounds like once the hub goes to suspend mode, the host is not responding to the wakeup when devices are inserted.
A USB host will typically put a hub in suspend mode when no downstream devices are connected to conserve power and enable the hub for remote wake. For some reason, it appears that the host is either not enabling remote wake or is not responding to the remote wake from the hub.
You can verify that the hub is sending the correct signaling by checking the upstream DP/DM lines, but I don't have a way to confirm the host behavior without a protocol analyzer. There were Linux builds with a remote wake issue several years ago, but I do not recall the build.
Regards,
JMMN