Part Number: DP83867CR
Other Parts Discussed in Thread: DP83867IS, DP83867IR,
DP83867IS(RGZ-48) can be both SGMII or RGMII based on strap/register settings.
So if the device was configured for RGMII-mode, would you be able to replace it with DP83867IR(RGZ-48)?
The pin layout seems identical (for RGMII use-case), and the register settings for "IR" device just has "Reserved" for all SGMII-related bits...it looks completely P2P compatible...
Can you confirm for me the following?
External Pinout:
1) Are DP83867IS (CS) and DP83867IR (CR) physically P2P compatible, if both are used for RGMII-interface? (external connections would be identical)
Internal Settings / STRAP config
2) All DP83867IS register settings related to SGMII seem to be "Reserved" bits in DP83867IR.
But, I noticed some registers like RGMIICTL2 are a little different (DP83867IS has a few more options)
Is it still possible, with minimal software modifications, to have a hardware P2P setup, and depending on the register settings used, also a software P2P configuration?
Darren