Part Number: DS90UB947-Q1
Hi team,
customer use 947+948, the back channel frequency is 20Mbps. they found that the 947+948 unlock when work in 20Mbps, and no display. If they pull down PDB then pull up, it also can lock and display normal.
Then, they set to 5Mbps of back channel in 948 side, the 947+948 can lock and display normally.
1. we would like to know why the 5Mbps can work while 20M not? which register can be used to monitor? my understanding is that, for 5Mbps and 20Mbps, the difference is CRC error. how many CRC error will cause lost lock? The CRC error of 5M should be less than 20Mbps.
2. In additional, in old 947 d/s, the 0x01 bit 7 is the auto sleep enable or disable. in the new d/s, the 0x01 bit 7 is reserved. We want to know that for 0x01 bit 7, it is still work for disable auto sleep AND just not open to customer or the 947 don't have auto sleep function? I ask this because in another project, also with 20Mbps back channel frequency, they enable the auto sleep, found 20Mbps can't lock. if they disable auto sleep, 20Mbps can work and display normal. but in this project, they set 0x01=00, it still unlock, only change to 5M or reset PDB.
thank you.