Hello,
What I want to do is to connect multiples boards (2 to 4) same way we usually do with RS485.
What is needed is a LVDS transceiver with a High Z output (an output enable).
Signals are coming from MOSI of SPI devices of the connected boards, going to the processor.
So when CSn is low the transceiver should be Low Z and High Z when high.
Is kind of IC exists?
Thank you.
Serge