This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261: Is it possible to program SPI Flash via USB Hub?

Guru 29720 points

Part Number: TUSB9261
Other Parts Discussed in Thread: TUSB8020B

Hi Team,

Is it possible to program SPI Flash of TUSB9261 under the below constitution with TUSB926x FlashBurner?
I assume windows PC is connected to USB Type-A in this case.
Is it possible to program via USB Hub (TUSB8020B)?

USB Type-A --- TUSB8020B --- TUSB9261 --- SSD
                                               |
                                               -- SOM

Best Regards,
Yaita