Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: TUSB1210 High-speed Detection Handshake Fail

Part Number: TUSB1210

Hi, 

We are develop a USB device and ULPI interface is used. We tested our RTL in FPGA and using ULPI PHY (TUSB1210).

But we found high-speed detection handshake is not successful. When USB device send TX CMD (84  54) and TX CMD (40 00) to ULPI PHY to let it to send Chirp K,

then, USB device waits for Chirp K/J/K/J/K/J from usb host, but there is no Chirp K/J/K/J/K/J received. 

The internal signal is shown as following figure(TX CMD (84 54) and TX CMD (40 00) are send to TUSB1210):

And we tested the signal of D+/D- after plugging USB cable to TSUB1210. It shows that signals keep toggling and this toggling is driven by TUSB1210.

The signals of D+/D- is shown in following figures:

From above, the amplitude of D- is larger than D+, this is a kind of strange.

So, do you have any suggestion for above testing result? I am looking forward to you reply.

Thanks and Best Regards,

Long