Part Number: LMH0302
Other Parts Discussed in Thread: LMH0397
Can I use LMH0302 to drive a cable when the input is a singled ended 75 ohm input? Leave SDI# floating or terminate it with a 75 ohm to ground? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tran,
I see two issues with your approach:
1). LMH0302 input is differential 100-ohm or single ended 50-ohm input.
2). LMH0302 is like a buffer or 75-ohm driver. It does not clean up any non-ideality due to signal integrity issues on its input. Therefor you would not get a clean signal on it's input. I don't know your application but you can use LMH0397 to receive from 75-ohm signal and transmit out on 75-ohm output as well.
Regards,, Nasser