Part Number: DS90UB953A-Q1
Hi,
In DS90UB953A-Q1 datasheet,
- Section 7.7.87-> What does CNTRL_ERR_HSRQST_CK0 error mean? When does it get asserted?
- Section 7.7.88-> Does this refer to datatype? If yes, I have multiple datatype in one frame so which data type gets reflected in this register
- Section 7.7.84-> LINE_LEN_MISMATCH -> is asserted when the amount of data received is less. similarly do we have an error indication when number of pixels received is more
- Do we have option to set line rate/resolution, framerate via register settings for the serializer?