Part Number: DS90UB954-Q1
Hi Team,
We saw two POC circuit in datasheet. Here are two questions.
- Why sometimes use 1*RL and sometimes 2*RL?
- Customer need more specific to the requirements of component parameters, such as SRF requirements, inductor's S-parameters in particular. Customer tested the 47uH inductor of Murata. According to their S-parameter simulation tool, it should be no problem. However, they found that there is a discrepancy. Originally, both S11 and S21 reserved a large margin, but it still couldn't meet the requirements.