Part Number: DP83826I
Helo E2E,
The CRS / LED3 pin is set to LED3 in ENHANCED mode.
LEDCFG Register (Address = 0x460) [reset = 0x650]
I set "LED3 Control" to 0x0, but it stays lit when the cable is unplugged.
The LED is on even though it is not LINK.
-> I want to find out the reason.
The LEDCFG2 (0x469) register only describes LED1 and LED2, but when I set the value with the recognition that LED3 is there, it seems that the polarity of LED3 can be set.
Is it okay to use it?
Regards,
ACGUY