Part Number: TCAN1042HGV-Q1
Hi TI team,
We are currently working on a project that has a really tight sleep current requirement and we request your help in finding out leakage current from TCAN IC. During the sleep mode of our device, only the 3.3V supply will be present and the 5V supply will be inactive. STB will be set high during sleep mode.
On the datasheet of TCAN1042, we find that the standby supply current is 17uA max. But we would like to know the entire current (supply + leakage currents) of TCAN when only the VIO supply is present and VCC is loaded as shown in the snippet below

If possible can you share the internal body structure of TCAN1042 IC? It would help us a lot in the assessment of sleep currents on the CAN section of our board.