Part Number: TPS65988DJEVM
Hello,
On the TPS65988EVM user guide schematic, Q16/Q18 looks to be a P channel MOSFET. However, on the BOM located in the TPS65988EVM user guide, Q16/Q18 is shown to be NX3008NBKW,115 which is a N-CH MOSFET. Typically, I would expect the current rating of the Q16/Q18 to be a minimum of 3 amps because USB charges between 3 to 5 amps, however, the NX3008NBKW has a 350mA rating. Is the BOM incorrect?
Thanks,
Michael