Part Number: DP83867E
Hi all,
I am using a DP83867E and attempting to use the BIST feature. I initialize the PHY with a reset and then simply enable the PRBS packet generator (reg 0x16 bit 12) with default values for IPG and packet length. I do not see the bytes received registers incrementing. Here is a dump of my registers after I end the BIST: Please note bit 14 in register 0x00 and bit 2 in register 0x16 are enabled (digital loopback enable).
| 0x00 | 0x00004000 |
| 0x01 | 0x00007949 |
| 0x02 | 0x00002000 |
| 0x03 | 0x0000a231 |
| 0x04 | 0x000001e1 |
| 0x05 | 0x00000000 |
| 0x06 | 0x00000064 |
| 0x07 | 0x00002001 |
| 0x08 | 0x00000000 |
| 0x09 | 0x00000300 |
| 0x0A | 0x00000000 |
| 0x0B | 0x00000000 |
| 0x0C | 0x00000000 |
| 0x0D | 0x0000401f |
| 0x0E | 0x0000f500 |
| 0x0F | 0x00003000 |
| 0x10 | 0x00005848 |
| 0x11 | 0x00000802 |
| 0x12 | 0x00000000 |
| 0x13 | 0x00000400 |
| 0x14 | 0x000029c7 |
| 0x15 | 0x00000000 |
| 0x16 | 0x00000004 |
| 0x17 | 0x00000040 |
| 0x18 | 0x00006150 |
| 0x19 | 0x00004444 |
| 0x1A | 0x00000002 |
| 0x1B | 0x00000000 |
| 0x1C | 0x00000000 |
| 0x1D | 0x00000000 |
| 0x1E | 0x00000002 |
| 0x1F | 0x00000000 |
| 0x25: | 0x00000400 |
| 0x2C: | 0x0000141f |
| 0x2D: | 0x00000000 |
| 0x2E: | 0x00000221 |
| 0x31: | 0x000010b0 |
| 0x32: | 0x000000d3 |
| 0x33: | 0x00000000 |
| 0x37: | 0x00000003 |
| 0x43: | 0x000007a0 |
| 0x53: | 0x00002055 |
| 0x55: | 0x00000000 |
| 0x6E: | 0x00000801 |
| 0x6F: | 0x00000100 |
| 0x71: | 0x00000000 |
| 0x72: | 0x00000000 |
| 0x7B: | 0x000005dc |
| 0x7C: | 0x0000007d |
| 0x86: | 0x00000077 |
| 0xC6: | 0x00000000 |
| 0xD3: | 0x00000000 |
| 0xE9: | 0x00009f22 |
| 0xFE: | 0x0000e721 |
| 0x12C: | 0x00000c2d |
| 0x134: | 0x00001000 |
| 0x135: | 0x00000000 |
| 0x136: | 0x00000000 |
| 0x137: | 0x00000000 |
| 0x138: | 0x00000000 |
| 0x139: | 0x00000000 |
| 0x13A: | 0x00000000 |
| 0x13B: | 0x00000000 |
| 0x13C: | 0x00000000 |
| 0x13D: | 0x00000000 |
| 0x13E: | 0x00000000 |
| 0x13F: | 0x00000000 |
| 0x140: | 0x00000000 |
| 0x141: | 0x00000000 |
| 0x142: | 0x00000000 |
| 0x143: | 0x00000000 |
| 0x144: | 0x00000000 |
| 0x145: | 0x00000000 |
| 0x146: | 0x00000000 |
| 0x147: | 0x00000000 |
| 0x148: | 0x00000000 |
| 0x149: | 0x00000000 |
| 0x14A: | 0x00000000 |
| 0x14B: | 0x00000000 |
| 0x14C: | 0x00000000 |
| 0x14D: | 0x00000000 |
| 0x14D: | 0x00000000 |
| 0x14E: | 0x00000000 |
| 0x14F: | 0x00000000 |
| 0x150: | 0x00000000 |
| 0x151: | 0x00000000 |
| 0x152: | 0x00000000 |
| 0x153: | 0x00000000 |
| 0x154: | 0x00000000 |
| 0x155: | 0x00000000 |
| 0x156: | 0x00000000 |
| 0x157: | 0x00000000 |
| 0x158: | 0x00000000 |
| 0x159: | 0x00000000 |
| 0x15A: | 0x00000000 |
| 0x15B: | 0x00000000 |
| 0x15C: | 0x00000000 |
| 0x15D: | 0x00000000 |
| 0x15E: | 0x00000000 |
| 0x15F: | 0x00000000 |
| 0x161: | 0x0000000c |
| 0x16F: | 0x00000095 |
| 0x170: | 0x00000c0b |
| 0x172: | 0x00000000 |
| 0x180: | 0x00000752 |
| 0x190: | 0x00000000 |
| 0x191: | 0x00000000 |
| 0x192: | 0x00000000 |
| 0x193: | 0x00000000 |
| 0x194: | 0x00000000 |
| 0x195: | 0x00000000 |
| 0x196: | 0x00000000 |
| 0x197: | 0x00000000 |
| 0x198: | 0x00000000 |
| 0x199: | 0x00000000 |
| 0x19A: | 0x00000000 |
| 0x19B: | 0x00000000 |
| 0x19C: | 0x00000000 |
| 0x19D: | 0x00000000 |
| 0x19E: | 0x00000000 |
| 0x19F: | 0x00000000 |
| 0x1A0: | 0x00000000 |
| 0x1A1: | 0x00000000 |
| 0x1A2: | 0x00000000 |
| 0x1A3: | 0x00000000 |
| 0x1A4: | 0x00000000 |
| 0x1D5: | 0x0000f500 |
Thanks in advance,
George