This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9546A: Component junction temperature spec. Tjmax( ℃ ) of TCA9546APWR

Genius 14500 points

Part Number: TCA9546A

Hi Team,


Could you assist to provide Component junction temperature spec. Tjmax( ℃ ) of TCA9546APWR?

Thank you.

william

  • Hi William,

    There are multiple ways that you calculate the junction temperature of a device. One equation is this one below:

    This report actually details many different equations that can be used to calculate the junction temperature.

    In general for logic devices the maximum junction temperature is equal to the maximum storage temperature. This is usually equal to 150 C. If you operate this device within the correct ambient temperature and within the absolute maximum ratings you don't have to worry about the junction temperature causing permanent damage to the device.

    Best,

    Chris