I currently have 2 boards using the P82B715 part to drive I2C over a cable (currently about 18"). The pull up on the "L" side is 330 ohms to +3.3V and on the "S" side is 1.8K to 3.3V. One of the boards has an AC input to an on-board AC-DC power supply which ultimately generates the 3.3V. The other board is powered by an off board AC-DC power supply that ultimately generates the 3.3V. My problem is that I'm not seeing any data on my oscope at the slave board. I measured the ground offset and it is about 3.2V--and when I connect the grounds from each board together, all the SCL lines (on both sides of each P82B715 device are pulled down to 109mV (master board), 180mV ("L" I2C line) and 235mV (slave board). Both boards measure 3.3V at their pull-up power supply test points. I feel like I am missing something stupid....