This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Question for FC GPIO EN option

Part Number: DS90UB953-Q1


Hi team,

Now I am supporting customer requirement for GPIO.

it is that

1) External Fsync from DES GPIO_0 to SER GPIO1.

2) Error flag from sensor need to be transfer from SER GPIO2 to DES GPIO1.

but when I refer to example script of 953/954 design guide, I need to set FC_GPIO_EN.

and now, customer requirement shows that SER GPIO2 need to use FC GPIO mode.

but 953/4 design guide says only GPIO_0 is available for 1ea FC GPIO mode.

Could you pls help me to know configuration how can I support my customer??

Thanks