This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: Camera link for EMC chamber

Part Number: DS90UB936-Q1

Device:  DS90UB936

End Equipment: camera link for EMC chamber

  1. On TX side, we are using just CML output from DS90UB936, therefore all CSI outputs are not used. For CSI port 1 we placed 100 Ohm termination, and for CSI port 2 we let open. Could you please confirm if is ok or not?
  2. For crystal oscillator we have used a simple 25Mhz Quartz. Is this fine? Or we should use a VCO oscillator?
  3. The POC filter. Could you please check if looks fine from technical point of view? Can we improve? Do you have suggestions?