Part Number: SN65LVELT22EVM
Other Parts Discussed in Thread: SN65LVELT22, DIP-ADAPTER-EVM
Hi Team,
My customer is asking for SN65LVELT22 Evaluation Module and as I check it seems to be not available.
Is there any similar/compatible evaluation board?
If none, I am thinking of suggesting a DIP-ADAPTER-EVM as a work around. Please see the link below:
DIP-ADAPTER-EVM Evaluation board | TI.com
My other problem with this is that as I check user guide. It only says that it supports SOIC-8 (U).
But I need to confirm if it also supports SOIC-8 (D) as it is the package of SN65LVELT22.
Also what is the difference between SOIC-8 (U) and SOIC-8 (D)?
Or is there a better work around than using DIP-ADAPTER-EVM?
I hope you can help me with this.
Thank you so much.
Gerald