Part Number: DS250DF410
Other Parts Discussed in Thread: DS280DF810
How do I write the register setting value when I want to use DS250DF410 with the configuration below?
rate : 25.78125Gbps

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS250DF410
Other Parts Discussed in Thread: DS280DF810
How do I write the register setting value when I want to use DS250DF410 with the configuration below?
rate : 25.78125Gbps

Hello Park,
Standard Data Rate Settings
The DS2x0DFx10 channels must each be preprogrammed for the expected data rate(s) to ensure CDR lock. Users can program the rate/sub-rate to one of a set of pre-defined standard values to quickly configure the DS2x0DFx10. The rate/sub-rate settings are programmed by writing to channel Reg_0x2F[7:4].
Table. Standard Rate Modes Configurable from Reg_0x2F
|
STANDARD RATE SETTING |
REG_0x2F VALUE [HEX] |
REG_0x2F WRITE MASK [HEX] |
|
10.3125 Gbps |
00 |
F0 |
|
10.9375 Gbps |
10 |
|
|
12.5 Gbps |
20 |
|
|
RESERVED |
30 |
|
|
25.0 Gbps |
40 |
|
|
25.78125 Gbps (default) |
50 |
|
|
RESERVED |
60 |
|
|
28.125 Gbps |
70 (DS280DF810 only) |
Regards,
Kia Rahbar