Part Number: TUSB1046-DCI
Hi,
I'm using TSB1046 and had a few questions as below for EQ settings. please kindly help on this.
1. DisplayPort Control(Did not see the register table corresponding to the EQ value)
For example, if my DP eq is to be changed to 7.5 dB, what value should I fill in?
0x10
0x11
2. USB3.1 Control(Did not see the register table corresponding to the EQ value)
For example, if my USB TX/RX eq is to be changed to 2.4/4.2 dB, what value should I fill in?
0x20
0x21