Part Number: XIO2001
Hi Team,
Customer is asking
1) Is attached reflow profile can be used for both IZGUR and IZWSR?
2) Do they share exact same solder ball material and foot print?
Thanks!
Andrew
TI Lead-free Reflow Profile Guideline.pdf

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: XIO2001
Hi Team,
Customer is asking
1) Is attached reflow profile can be used for both IZGUR and IZWSR?
2) Do they share exact same solder ball material and foot print?
Thanks!
Andrew
TI Lead-free Reflow Profile Guideline.pdf

Hi Andrew,
1). Given pkg thickness is less than 1.6mm, peak reflow is at 260degC as you noted. Please below note figure 3 for reflow profile:
2). Solder ball material and composition is the same.
Regards,, Nasser