Part Number: TUSB8041A
Hi,
I try to enable the TUSB8041As SMB interface. For that, I've connected the SMBUSZ pin with 40k resistor to ground. Is this correct? I'm asking because this way, I'm seeing the TUSB8041A pulling the SMBCLK and SMBDAT line beeing pulled to ~2V. At the same time I'm seeing ~300mA drawn on 1.1V line. The GRSTZ pin is held to ground over a 40k resistor all the time in this scenario.
I'm measuring ~3.2V at the SMBUSZ pin. Does that mean, that 40k is too large? If so, how to dimension the required a pull-down resistor for SMBUSZ?
Here is the schematic of the whole project: https://docs.google.com/viewer?url=http%3A%2F%2Fwww.mikrocontroller.net%2Fattachment%2F493708%2Fbase-plane.pdf the TUSB8041A is on page 5.
Thanks in advance for any help, suggestion, pointers etc.
Torsten