This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: DS90UB960-Q1 MIPI-CSI bandwidth

Part Number: DS90UB960-Q1

Hello,experts

I 'm using a DS90UB960 which is connected to four DS90UB953. Each DS90UB953 sends a 1920x 1080 x12bit x30fps video.System works in the Best-Effort Round Robin mode.

When I set DS90UB960 mipi csi in continuous clock mode (four lane , 1.6Gbps per lane), everything is OK. But when I set DS90UB960 mipi csi in discontinuous clock mode(four lane , 1.6Gbps per lane), I can't reveice correct video. So, is mipi csi discontinuous clock mode 's bandwidth enough for four 1920x 1080 x12bit x30fps video?

Best Regards

Nick