Part Number: TIOL1113
Hello,
I want to use the TIOL1113 at Ta = -40 .. +85°C. Io (lim) = 150mA. Io (nom) = 100mA. I have 2 questions regarding inductive loads:
1.) Figure 29 and 30 of the datasheet show that the internal circuit can demagnetize the 1.5H at a steady state current of Io = 240mA. So I assume that the circuit is safely capable of demagnetizing the energy at lower currents (100mA)?
2.) Is there any restiction in switching frequency due to medium power dissipation? For my application 2.5Hz would be sufficient.
Best regards,
Chris