Part Number: DP83848M
Other Parts Discussed in Thread: TIDA-00207
Hello,
I am using the DP83488 in a design and I am currently selecting the crystal. In order to verify that the selected crystal operates in its permitable power range, I need to calculate the crystal power dissipation value. For that I would need to know the voltage at which the crystal oscillator circuit operates (amplitude of the oscillation).
Pxtal = 0.5 ESR (2*π*frequency*CLoad*VDDS_OSC)²
If I take the crystal and components used in the TIDA-00207 I get for a voltage of 1.8V a drive level of 740uW, which is outside of the specification of the used crystal.
(CTS 445I23D25M00000 => ESR=40R; C0=5.0pF; CLoad=18pF; 300uW Max)
What is the crystal oscillator circuit voltage, resp. what is the amplitude of the oscillation?
Thanks a lot for your help,
have a nice day,
Bernd