Part Number: DP83826EVM
Other Parts Discussed in Thread: USB-2-MDIO
Dear Team,
Hello, I have some questions for you from DP83826EVM.
I want to check various signals while changing the register. I have checked up to register read and write through USB-2-MDIO.
1. In EVM, MAC Interface was set to MII, but if you want to check the waveform in RMII Slave mode, can you just change the register value?
Or is it necessary to connect a MAC capable of CLK output to the PHY? I'm not sure how exactly.
2. I want to proceed with the MII loopback test using the EVM kit. Can I just change the register of the relevant area and connect the LAN cable to RJ45 to proceed with the loopback test?
please answer about my question. Thank you.